Everything

csplus.get_timer_providers


This function gets the supported timer providers.

[Specification format]

csplus.get_timer_providers()

[Argument(s)]

None

[Return value]

A dictionary for the ID and name of the supported timer providers is returned.

Key : ID of the provider (This is fixed to 'csplus.timer' in this version.)

Value : Name of the provider (This is fixed to 'Time Measurement' in this version.)

[Detailed description]

-

This function gets the supported timer providers.

[Example of use]

>>> csplus.get_timer_providers()
{'csplus.timer': 'Time Measurement'}