csplus.select_timer_provider
|
This function specifies the timer provider which is to be used for timer-related functions.
[Specification format]
csplus.select_timer_provider(provider_id)
|
[Argument(s)]
|
|
provider_id
|
The ID of the timer provider is specified.
|
[Return value]
None
[Detailed description]
- | This function specifies the timer provider which is to be used for timer-related functions. |
[Example of use]
>>> csplus.get_timer_providers()
{'csplus.timer': 'Time Measurement'}
>>> csplus.select_timer_provider("csplus.timer")
|