|
build.Assemble.OutputAssembleListFile
|
This property is for setting or referring to whether to output assembly listing files. It is an assembly option for the active project.
[Specification format]
build.Assemble.OutputAssembleListFile = bool
|
[Setting(s)]
|
|
|
|
bool
|
Set whether to output assembly listing files.
True: Output assembly listing files.
False: Do not output assembly listing files.
|
[Reference]
If assembly listing files are to be output: True
If assembly listing files are not to be output: False
[Detailed description]
- | This property is for setting or referring to whether to output assembly listing files. It is an assembly option for the active project. |
[Example of use]
>>>build.Assemble.OutputAssembleListFile = True
>>>print build.Assemble.OutputAssembleListFile
True
>>>
|