|
build.Common.MergedErrorMessageFileOutputFolder
|
This property is for setting or referring to the folder for the output of error message merge files. It is a common option for the build tool for the active project. [CC-RH] [CC-RL]
[Specification format]
build.Common.MergedErrorMessageFileOutputFolder = folder
|
[Setting(s)]
|
|
|
|
folder
|
Set the path to the folder for the output of error message merge files as strings.
|
[Reference]
Path to the folder for the output of error message merge files
[Detailed description]
- | This property is for setting or referring to the folder for the output of error message merge files. It is a common option for the build tool for the active project. |
[Example of use]
>>>build.Common.MergedErrorMessageFileOutputFolder = "/ProjectDir/Output_Vx.xx.xx"
>>>print build.Common.MergedErrorMessageFileOutputFolder
%ProjectDir%\Output_Vx.xx.xx
>>>
|