This property is for setting or referring to the precision of double type and long double type. It is a compile option for the active project. [CC-RH V1.02.00 and later versions]
|
Handles double type and long double type as single-precision floating-point type (4 bytes). |
||
|
Handles double type and long double type as double-precision floating-point type (8 bytes). |
||
This property is for setting or referring to the precision of double type and long double type. It is a compile option for the active project. |