Everything
 

[Text Editor - Encoding] category


Use this category to configure general settings relating to the text editor.

Figure A.53

Option Dialog Box ([Text Editor - Encoding] Category)

 

The following items are explained here.

[How to open]

-

From the [Tool] menu, select [Options...].

[Description of each area]

(1)

[Encoding]

Use this area to make the settings related to the encoding used in the text editor.

(a)

[Enable file encoding auto detection]

 

Enables automatic detection of the encoding when a file is read (default).

 

Disables automatic detection of the encoding when a file is read.

(b)

[Prefer Default file encoding if auto detection is failed]

This item is only enabled when the [Enable file encoding auto detection] check box is selected.

 

The default encoding takes precedence if automatic detection was not possible.

 

The default encoding does not take precedence if automatic detection was not possible (default).

Remark

If automatic detection does not obtain the expected encoding, changing the setting of this option may improve the situation.

(c)

[Default file encoding]

This option is for the default file encoding that should be used when creating a new file in the Editor panel and automatic detection of encoding is disabled. In addition this encoding is used when the file being opened has a file encoding that cannot be detected or is not supported in the Editor panel currently.

Select the encoding to be set from the drop-down list.

The items of the drop-down list are displayed according to the following sequence.

Note that the same encoding and encoding which are not supported by the current OS will not be displayed.

-

Default encoding of the current OS (default)

-

Most recently used encodings (maximum 4)

-

Popular encodings for current locale
e.g. for United States locale it will be:

-

Western European (Windows)

-

Unicode (UTF-8)

-

All other encodings supported by the OS (in alphabetical order)

Caution 1.

If you wish to select a different encoding in the text editor and save the file, use [Target Save Option...] of the [File] menu for the editing file. Note that [Default file encoding] does not override the setting.

Caution 2.

If you wish to make an encoding setting specific to building, modify the corresponding property of the build tool listed in the tables below, respectively. Note that [Default file encoding] does not override these settings.

Compiler Package

Property Of Build Tool

CC-RH

[Character encoding] property in the [Character Encoding] category from the [Compile Options] tab or [Individual Compile Options] tab

[Character encoding] property in the [Character Encoding] category from the [Assemble Options] tab or [Individual Assemble Options] tab

CC-RX

[Character code of an input program] property in the [Source] category from the [Compile Options] tab, [Individual Compile Options(C)] tab, or [Individual Compile Options(C++)] tab

[Character code of an output assembly-language file] property in the [Object] category from the [Compile Options] tab, [Individual Compile Options(C)] tab, or [Individual Compile Options(C++)] tab

[Character code of an input program] property in the [Source] category from the [Assemble Options] tab or [Individual Assemble Options] tab

CC-RL

[Character encoding] property in the [Character Encoding] category from the [Compile Options] tab or [Individual Compile Options] tab

[Character encoding] property in the [Character Encoding] category from the [Assemble Options] tab or [Individual Assemble Options] tab

(2)

Buttons

Initialize Settings

Returns all currently displayed setting to their default values.

[Function buttons]

Button

Function

Initialize All Settings

Restores all settings on this dialog box to their default values.

Note, however, that newly added items in the [General - External Tools] category will not be removed.

OK

Applies all setting and closes this dialog box.

Cancel

Ignores the setting and closes this dialog box.

Apply

Applies all setting (does not close this dialog box).

Help

Displays the help of this dialog box.