This dialog box reads the analysis information saved as task analyzer trace data and displays the information in the Child-panel display area on the Realtime OS Task Analyzer panel.
The following items are explained here.
Select [Opens trace data...] from the menu list located on the Toolbar on the Realtime OS Task Analyzer panel. |
Selects a folder containing the task analyzer trace data.
Lists the files that meet the conditions selected in [Look in] and [Files of type].
Specifies the name of the file containing the task analyzer trace data to be read.
Selects "Task analyzer trace data (*.tad)" as the type of the file to be read.
|
From the folder specified in [Look in], read the file specified in [File name] and [Files of type] to display the applicable information on the Analysis Result panel. |
|