You can save the contents of the Function List panel, Variable List panel, Analysis Chart panel, Call Graph panel, and Variable Value Changing Chart (zoomed in) panel to a file.
To do this, with the focus on the Function List panel, select [Save Function List Data As...] from the [File] menu. The Save As dialog box opens; perform the operation from this dialog.
The following file formats can be specified when saving the information.
|
File format to import the function information (see "2.12Import or Export Information File".) |
To do this, with the focus on the Variable List panel, select [Save Variable List Data As...] from the [File] menu. The Save As dialog box opens; perform the operation from this dialog.
The following file formats can be specified when saving the information.
|
File format to import the variable information (see "2.12Import or Export Information File".) |
To do this, with the focus on the Analysis Chart panel, select [Save Analysis Chart Data As...] from the [File] menu, or with the focus on the Variable Value Changing Chart (zoomed in) panel, click the [Save] button. The Save As dialog box opens; perform the operation from this dialog.
The following file formats can be specified when saving the information.
This format is only applied to the [Variable Value Changing Chart] tab of the Analysis Chart panel. |
Only the area of graph rendering is saved (trigger marks, channel information, etc. cannot be saved). |
For the Analysis Chart panel, only the contents of the currently displayed tab will be saved. |
When the graphic file format is selected, only the part currently being displayed in the panel will be saved. |
To do this, with the focus on the Call Graph panel, select [Save Call Graph Data As...] from the [File] menu. The Save As dialog box opens; perform the operation from this dialog.
The following file formats can be specified when saving the information.
Note that when "(Only the visible part)" is selected, only the part currently being displayed in the panel will be saved.
All part of the call graph may not successfully be saved as a graphic file format if the project is too big. |