|
Target range
|
Specifies the target range.
Specifies in the format of "start address-end address" or "section name".
Specifies an address in the hexadecimal notation (example: 400-ffff).
The range of specifiable address values is 0 to FFFFFFFF
This property corresponds to the -crc option of the linker.
|
|
Default
|
Target range[number of defined items]
|
|
How to change
|
Directly enter in the text box or edit by the Character String Input dialog box which appears when clicking the [...] button.
|
|
Restriction
|
Up to 32767 characters
Up to 65536 items can be specified.
|
|
Type of CRC
|
Selects the method of CRC operation.
See the user's manual of the device and "CC-RX Compiler User's Manual" for details about each operation.
This property corresponds to the -CRc option of the linker.
|
|
Default
|
CCITT type
|
|
How to change
|
Select from the drop-down list.
|
|
Restriction
|
CCITT type
|
Outputs the calculation result of CRC-16-CCITT-MSB first operation with an initial value of 0xffff and inverse of XOR.
|
|
16
|
Outputs the calculation result of CRC-16-LSB first operation.
|
|
CRC-CCITT(MSB) type
|
Outputs the calculation result of CRC-16-CCITT-MSB first operation.
|
|
CRC-CCITT(MSB,LITTLE,4 bytes) type
|
Outputs the calculation result of CRC-16-CCITT-MSB first operation with the input specified as 4-byte units in little-endian mode.
|
|
CRC-CCITT(MSB,LITTLE,2 bytes) type
|
Outputs the calculation result of CRC-16-CCITT-MSB first operation with the input specified as 2-byte units in little-endian mode.
|
|
CRC-CCITT(LSB) type
|
Outputs the calculation result of CRC-16-CCITT-LSB first operation.
|
|
SENT(MSB) type
|
Outputs the calculation result of operation conforming to SENT.
|
|
32-ETHERNET type
|
Outputs the calculation result of CRC-32-ETHERNET operation.
|
|
Initial value
|
Specifies the initial value for the CRC operation in the format of "initial value".
This property corresponds to the -CRc option of the linker.
|
|
Default
|
Blank
|
|
How to change
|
Directly enter to the text box.
|
|
Restriction
|
- | When other than [32-ETHERNET type] is selected in the [Type of CRC] property |
0 to FFFF (hexadecimal number)
- | When [32-ETHERNET type] is selected in the [Type of CRC] property |
0 to FFFFFFFF (hexadecimal number)
|
|
Endian
|
Selects the endian for CRC output.
This property corresponds to the -CRc option of the linker.
|
|
Default
|
Not specify
|
|
How to change
|
Select from the drop-down list.
|
|
Restriction
|
Not specify
|
Does not specify the endian. Depends on the endian type of the input object.
|
|
Little endian
|
Outputs the value in little-endian mode.
|
|
Big endian
|
Outputs the value in big-endian mode.
|
|
Output size
|
Specifies the output size for the CRC code.
This property corresponds to the -CRc option of the linker.
|
|
Default
|
Blank
|
|
How to change
|
Directly enter to the text box.
|
|
Restriction
|
2, 4, or blank
|