This section explains CcnvCA78K0R options.
 
-  | Uppercase characters and lowercase characters are distinguished for options.  | 
 
-  | When a file name is specified as a parameter, it can include the path (absolute path or relative path). When a file name without the path or a relative path is specified, the reference point of the path is the current folder.   | 
 
-  | When a parameter includes a space (such as a path name), enclose the parameter in a pair of double quotation marks (").  | 
 
 
| 
 | 
 | 
| 
 
-V 
 | 
 
This option displays the version information of CcnvCA78K0R. 
 | 
| 
 
-h 
 | 
 
This option displays the descriptions of CcnvCA78K0R options. 
 | 
| 
 
-c 
 | 
 
This option specifies the Japanese character code. 
 | 
| 
 
-l 
 | 
 
This option specifies the list file name. 
 | 
| 
 
-o 
 | 
 
This option specifies the output file name. 
 | 
| 
 
-r 
 | 
 
This option specifies where the message is to be output. 
 | 
| 
 
-A 
 | 
 
This option performs conversion with the functions related to the ANSI standard enabled. 
 |