Reads the results of A/D conversion (12 bits).
[Syntax]
#include "r_cg_macrodriver.h"
MD_STATUS R_12ADC_Get_ValueResult ( ad_channel_t channel, uint16_t * const buffer );
[Argument(s)]
| I/O | Argument | Description | 
| I | ad_channel_t channel; | Analog voltage input pin | 
| O | uint16_t * const buffer; | Pointer to area in which to store read results of A/D conversion | 
[Return value]
| Macro | Description | 
| MD_OK | Normal completion | 
| MD_ARGERROR | Invalid argument specification |