Usage example (Phase counting mode)
A phase difference between external input signals from two pins TRGCLKA and TRGCLKB is detected and the TRG register is incremented/decremented.
Count the number of TRG register overflow and underflow.
[Waveform example]

[GUI setting example]
| 
       TimerRG  | 
    
       Used  | |||
| 
       TMRG  | 
    
       Used  | |||
| 
       Functions  | 
    
       Phase counting mode  | |||
| 
       Initial count  | 
    
       0  | |||
| 
       Counter clear  | 
    
       Clear disabled  | |||
| 
       CNTEN0  | 
    
       Used  | |||
| 
       CNTEN1  | 
    
       Used  | |||
| 
       CNTEN2  | 
    
       Used  | |||
| 
       CNTEN3  | 
    
       Used  | |||
| 
       CNTEN4  | 
    
       Used  | |||
| 
       CNTEN5  | 
    
       Used  | |||
| 
       CNTEN6  | 
    
       Used  | |||
| 
       CNTEN7  | 
    
       Used  | |||
| 
       Enable TRG overflow interrupt  | 
    
       Used  | |||
| 
       Enable TRG under flowinterrupt  | 
    
       Used  | |||
| 
       INTTRG priority  | 
    
       Low/ level3 (low priority level)  | |||
[API setting example]
r_cg_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start the TMRG module operation */
R_TMRG0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_tmrg_user.c
/* Start user code for global. Do not edit comment generated here */
volatile uint8_t inttrg_over_cnt = 0U;
volatile uint8_t inttrg_under_cnt = 0U;
/* End user code. Do not edit comment generated here */
static void __near r_tmrg0_interrupt(void)
{
/* Start user code. Do not edit comment generated here */
uint8_t temp_trg = 0U;
/* === Count number of overflow or under flow === */
/* Mask TRGSR resister to check overflow or underflow occurred */
temp_trg = TRGSR & 0x0CU;
if (temp_trg == 0x08U)
{
/* --- Count up number of overflow --- */
inttrg_over_cnt++;
/* --- Clear overflow Flag --- */
TRGSR &= 0x07U;
}
else
{
/* --- Count up number of underflow --- */
inttrg_under_cnt++;
/* --- Clear under flow Flag --- */
TRGSR &= 0x0BU;
}
/* End user code. Do not edit comment generated here */
}