Serial communications interface (SCI)
Below is a list of API functions output by the Code Generator for serial communications interface use.
Table 3.25 API Functions: [Serial Communications Interface]
|
API Function Name |
Function |
|
Performs initialization necessary to control the serial communications interface. | |
|
Performs user-defined initialization related to the serial communications interface. | |
|
Performs processing in response to the transmit-end interrupts. | |
|
Performs processing in response to the transmit-data-empty interrupts. | |
|
Performs processing in response to the receive-data-full interrupts. | |
|
Performs processing in response to the receive error interrupts. | |
|
Starts SCI communication. | |
|
Ends SCI communication. | |
|
Starts SCI transmission (synchronous mode). | |
|
Starts SCI reception (synchronous mode). | |
|
Starts SCI transmission (multi-processor communications function). | |
|
Starts SCI reception (multi-processor communications function). | |
|
Starts SCI transmission/reception (clock synchronous mode). | |
|
Starts SCI transmission (smart card interface mode). | |
|
Starts SCI reception (smart card interface mode). | |
|
Starts SCI master transmission (simple I2C mode). | |
|
Starts SCI master reception (simple I2C mode). | |
|
Starts SCI master transmission (simple SPI mode). | |
|
Starts SCI master transmission/reception (simple SPI mode). | |
|
Starts SCI slave transmission (simple SPI mode). | |
|
Starts SCI slave transmission/reception (simple SPI mode). | |
|
Sends the start bit. | |
|
Sends the stop bit. | |
|
Performs processing in response to the transmit-end interrupts. | |
|
Performs processing in response to the receive-data-full interrupts. | |
|
Performs processing in response to the receive error interrupts. |