Following is the rules for input to the Peripheral Functions panel.
Character sets that are allowed to input are as follows.
|
ASCII
|
1-byte alphabet, number, symbol
|
|
Shift-JIS
|
2-byte alphabet, number, symbol, Hiragana, Katakana, Kanji and 1-byte Katakana
|
|
EUC-JP
|
2-byte alphabet, number, symbol, Hiragana, Katakana, Kanji and 1-byte Katakana
|
|
UTF-8
|
2-byte alphabet, number, symbol, Hiragana, Katakana, Kanji (include Chinese character) and 1-byte Katakana
|
Notations allowed when entering numbers are as follows.
|
Decimal number
|
A numeric value that starts with a number between 1 and 9 and followed by numbers between 0 and 9, and the numeric value 0
|
|
Hex number
|
A numeric value that starts with 0x and followed by a combination of numbers from 0 to 9 and characters from A to F (characters are not case sensitive)
|