-
[ RI600PX ] tab
-
This tab shows the detailed information on RI600PX to be used categorized by the following.
1 ) [Version Information]
The detailed information on the version of the RI600PX are displayed.
|
|
Display the version of RI600PX to be used.
|
|
|
The version of the installed RI600PX
|
|
|
|
|
|
Display the folder in which RI600PX to be used is installed with the absolute path.
|
|
|
The folder in which RI600PX to be used is installed
|
|
|
|
|
|
Display the endian set in the project.
Display the same value as the value of the [Select endian] property of the build tool.
|
|
|
The endian in the property of the build tool
|
|
|
|