-
tloc_mtx
-
Lock mutex (with time-out).
ER tloc_mtx (ID mtxid, TMO tmout);
|
|
|
|
|
|
ID mtxid;
|
|
|
|
TMO tmout;
|
Specified time-out (in millisecond).
Value: Specified time-out.
|
This service call locks the mutex specified by parameter
mtxid.
If the target mutex could not be locked (another task has been locked) when this service call is issued, this service call queues the invoking task to the target mutex wait queue and moves it from the RUNNING state to the WAITING state with time-out (mutex wait state).
The WAITING state for a mutex is cancelled in the following cases.
WAITING State for a Mutex Cancel Operation
|
|
The locked state of the target mutex was cancelled as a result of issuing unl_mtx.
|
|
The locked state of the target mutex was cancelled as a result of issuing ext_tsk.
|
|
The locked state of the target mutex was cancelled as a result of issuing exd_tsk.
|
|
The locked state of the target mutex was cancelled as a result of issuing ter_tsk.
|
|
Forced release from waiting (accept rel_wai while waiting).
|
|
Forced release from waiting (accept irel_wai while waiting).
|
|
The time specified by tmout has elapsed.
|
|
Forced release from waiting (accept del_mtx while waiting).
|
|
When the mutex is locked, this service call changes the current priority of the invoking task to the ceiling priority of the target mutex. However, this service call does not change the current priority when the invoking task has locked other mutexes and the ceiling priority of the target mutex is lower than or equal to the ceiling priority of the locked mutexes.
Note 1 Invoking tasks are queued to the target mutex wait queue in task current priority order. Among tasks with the same priority, they are queued in FIFO order.
Note 2 This service call returns "E_ILUSE" if this service call is re-issued for the mutex that has been locked by the invoking task (multiple-locking of mutex).
Note 3
TMO_FEVR is specified for wait time
tmout, processing equivalent to
loc_mtx will be executed. When
TMO_POL is specified, processing equivalent to
ploc_mtx will be executed.
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
- This service call was issued from a non-task.
- This service call was issued in the CPU locked state.
- This service call was issued in the dispatching disabled state.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
|
|
|
|
- Stack pointer points out of user stack for invoking task.
|
|
|
|
Illegal use of service call.
- The invoking task has already locked the target mutex.
- Ceiling priority violation (the base priority of the invoking task < the ceiling priority of the target mutex)
|
|
|
|
- The mutex specified by mtxid does not exist.
|
|
|
|
Forced release from the WAITING state.
|
|
|
|
Polling failure or specified time has elapsed.
|
|
|
|
|