-   
   dly_tsk
  
    -   
  
 ER      dly_tsk (RELTIM dlytim);
 
  
  
    |  |  |  | 
  
    |  | 
 RELTIM  dlytim;
 | 
 Amount of time to delay the invoking task (in millisecond).
 | 
 
 This service call moves the invoking task from the RUNNING state to the WAITING state (delayed state).
 
 As a result, the invoking task is unlinked from the ready queue and excluded from the RI600V4 scheduling subject.
 
 The delayed state is cancelled in the following cases.
 
  
  
  
    | 
 Delayed State Cancel Operation
 |  | 
  
    | 
 Delay time specified by parameter dlytim  has elapsed.
 |  | 
  
    | 
 Forced release from waiting (accept rel_wai  while waiting).
 |  | 
  
    | 
 Forced release from waiting (accept irel_wai  while waiting).
 |  | 
 
 Note	 When 0 is specified as 
dlytim, the delay time is up to next base clock interrupt generation. 
 
 
  
  
    |  |  |  | 
  
    |  |  |  | 
  
    |  |  |  | 
  
    |  |  | 
 -	 This service call was issued from a non-task.
 
 -	 This service call was issued in the CPU locked state.
 
 -	 This service call was issued in the dispatching disabled state.
 
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
 | 
  
    |  |  | 
 Forced release from the WAITING state.
 |