vrst_mpl
ER vrst_mpl (ID mplid);
 The tasks to wait to get memory block from the target variable-sized memory pool are released from the WAITING state, and EV_RST is returned as a return value for the tasks.
 Note 1	 All variable-sized memory blocks that had already been acquired are returned to the target variable-sized memory pool. Therefore, do not access those variable-sized memory blocks after issuing this service call.