13.4.7 Cyclic handler information
 The number of cyclic handler information items that can be specified is defined as being within the range of 0 to 127.
 Note The CF78V4 outputs to the system information header file the correspondence between the cyclic handler names and IDs, in the following format. Consequently, cyclic handler names can be used in the place of IDs by including the relevant system information header file using the processing program.
 Specifies the attributes (coding language, initial activation status) of the cyclic handler.
The keywords that can be specified for cycatr are TA_HLNG, TA_ASM and TA_STA, TA_PHS.
The keywords that can be specified for cycatr are TA_HLNG, TA_ASM and TA_STA, TA_PHS.
 Note If specification of TA_STA is omitted, the cyclic handler initial activation status is set to "non-operational state (STP state)".
 Specifies the start address of the cyclic handler.
Values that can be specified for cychdr are symbol names written in C.
Values that can be specified for cychdr are symbol names written in C.
 Note 1	 When the cyclic handler is in written in C as shown below, the value specified by this item is "func_cychdr".
 Note 2	 When the cyclic handler is in written in assembly language as shown below, the value specified by this item is "func_cychdr".
$INCLUDE (kernel.inc) $INCLUDE (kernel_id.inc) .PUBLIC _func_cychdr .SECTION .text, TEXT _func_cychdr: ; ............ RET  | 
  
 Specifies the activation cycle (unit: ticks) of the cyclic handler.
A value between 1 and 4294967295 can be specified for cyctim.
A value between 1 and 4294967295 can be specified for cyctim.
 Specifies the activation phase (in millisecond) for a cyclic handler.
A value from 0x1 to 0x7fffffff (aligned to `clkcyc' multiple values) can be specified for cycphs.
A value from 0x1 to 0x7fffffff (aligned to `clkcyc' multiple values) can be specified for cycphs.
 Note 1	 In the RI78V4, the initial activation phase means the relative interval from when generation of s cyclic handler is completed until the first activation request is issued.
 Note 2	 If a value other than an integral multiple of the base clock cycle defined in Clock timer interrupt source is specified for cycphs, the CF78V4 assumes that an integral multiple is specified and performs processing.