get_mpf
 This service call acquires the memory block from the fixed-sized memory pool specified by parameter mpfid and stores the start address in the area specified by parameter p_blk.
 If a memory block could not be acquired from the target fixed-sized memory pool (no available memory blocks exist) when this service call is issued, memory block acquisition processing is not performed but the invoking task is queued to the target fixed-sized memory pool wait queue in the order of memory block acquisition request (FIFO order).
 As a result, the invoking task is unlinked from the ready queue and is moved from the RUNNING state to the WAITING state (waiting state for a fixed-sized memory block).
 The waiting state for a fixed-sized memory block is cancelled in the following cases, and then moved to the READY state.