sta_cyc
 This service call moves the cyclic handler specified by parameter cycid from the non-operational state (STP state) to operational state (STA state).
 Note This service call does not perform queuing of start requests. If the target cyclic handler has been moved to the operational state (STA state), only activation cycle re-set processing is executed.
The relative time interval from the output of this service call until the first activation request is output is always the activation phase (activation cycle cyctim) using the output of this service call as the reference point.
The relative time interval from the output of this service call until the first activation request is output is always the activation phase (activation cycle cyctim) using the output of this service call as the reference point.