set_flg
iset_flg
ER set_flg (ID flgid, FLGPTN setptn);
ER iset_flg (ID flgid, FLGPTN setptn);
 These service calls set the result of logical OR operating the bit pattern of the eventflag specified by parameter flgid and the bit pattern specified by parameter setptn as the bit pattern of the target eventflag.
 If the required condition of the task queued to the target eventflag wait queue is satisfied when this service call is issued, the relevant task is unlinked from the wait queue at the same time as bit pattern setting processing.
 As a result, the relevant task is moved from the WAITING state (WAITING state for an eventflag) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
 Note 1	 If the bit pattern set to the target eventflag is B'1100 and the bit pattern specified by parameter setptn is B'1010 when this service call is issued, the bit pattern of the target eventflag is set to B'1110.
 Note 2	 When the TA_WMUL attribute is specified for the target eventflag, the range of tasks to be checked on "whether issuing of this service call satisfies the required condition" differs depending on whether the TA_CLR attribute is also specified.