sta_cyc
ista_cyc
ER sta_cyc (ID cycid);
ER ista_cyc (ID cycid);
 This service call moves the cyclic handler specified by parameter cycid from the non-operational state (STP state) to operational state (STA state).
 The relative interval from when either of this service call is issued until the first activation request is issued varies depending on whether the TA_PHS attribute is specified for the target cyclic handler during configuration.
 -	 If the TA_PHS attribute is specified
The target cyclic handler activation timing is set based on the activation phases (initial activation phase cycphs and activation cycle cyctim) defined during configuration.
If the target cyclic handler has already been started, however, no processing is performed even if this service call is issued, but it is not handled as an error.
The target cyclic handler activation timing is set based on the activation phases (initial activation phase cycphs and activation cycle cyctim) defined during configuration.
If the target cyclic handler has already been started, however, no processing is performed even if this service call is issued, but it is not handled as an error.