-   
 
   trcv_dtq
  
    -   
  
 
 Receive from data queue (with timeout).
 
 ER      trcv_dtq (ID dtqid, VP_INT *p_data, TMO tmout);
 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 ID      dtqid;
 
 | 
    
 ID number of the data queue from which a data element is received.
  
 | 
  
  
    | 
 | 
    
 VP_INT  *p_data;
 
 | 
    
 Data element received from the data queue.
  
 | 
  
  
    | 
 | 
    
 TMO     tmout;
 
 | 
    
 Specified timeout (unit:millisecond).
  
 TMO_FEVR:	Waiting forever.
  
 Value:	Specified timeout.
  
 | 
  
 
 This service call reads data in the data queue area of the data queue specified by parameter 
dtqid and stores it to the area specified by parameter 
p_data.
 
 If no data could be read from the data queue area of the target data queue (no data has been written to the data queue area) when this service call is issued, the service call does not read data but queues the invoking task to the reception wait queue of the target data queue and moves it from the RUNNING state to the WAITING state with time out (data reception wait state).
 
 The receiving WAITING state for a data queue is cancelled in the following cases, and then moved to the READY state.
 
  
  
  
    
 Receiving WAITING State for a Data Queue Cancel Operation
  
 | 
    
 | 
  
  
    
 Data was written to the data queue area of the target data queue as a result of issuing  snd_dtq.
  
 | 
    
 | 
  
  
    
 Data was written to the data queue area of the target data queue as a result of issuing  psnd_dtq.
  
 | 
    
 | 
  
  
    
 Data was written to the data queue area of the target data queue as a result of issuing  ipsnd_dtq.
  
 | 
    
 | 
  
  
    
 Data was written to the data queue area of the target data queue as a result of issuing  tsnd_dtq.
  
 | 
    
 | 
  
  
    
 Data was written to the data queue area of the target data queue as a result of issuing  fsnd_dtq.
  
 | 
    
 | 
  
  
    
 Data was written to the data queue area of the target data queue as a result of issuing  ifsnd_dtq.
  
 | 
    
 | 
  
  
    
 Forced release from waiting (accept  rel_wai while waiting).
  
 | 
    
 | 
  
  
    
 Forced release from waiting (accept  irel_wai while waiting).
  
 | 
    
 | 
  
  
    
 Polling failure or timeout.
  
 | 
    
 | 
  
 
 Note 1	 Invoking tasks are queued to the reception wait queue of the target data queue in the order of the data reception request.
 
 Note 2	 If the data reception wait state is cancelled because 
rel_wai or 
irel_wai was issued or the wait time elapsed, the contents in the area specified by parameter 
p_data become undefined.
 
 Note 3	 TMO_FEVR is specified for wait time 
tmout, processing equivalent to 
rcv_dtq will be executed. When TMO_POL is specified, processing equivalent to 
prcv_dtq /
iprcv_dtq will be executed.
 
 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 | 
    
 -	  dtqid > Maximum ID number
  
 | 
  
  
    | 
 | 
    
 | 
    
 -	 This service call was issued from a non-task.
  
 -	 This service call was issued in the CPU locked state.
  
 -	 This service call was issued in the dispatching disabled state.
  
 | 
  
  
    | 
 | 
    
 | 
    
 -	 Specified data queue is not registered.
  
 | 
  
  
    | 
 | 
    
 | 
    
 Forced release from the WAITING state.
  
 | 
  
  
    | 
 | 
    
 | 
    
 -	 Polling failure or timeout.
  
 |