This option performs optimization assuming that the files to be compiled comprise the entire program.
It is not assumed that the files to be compiled comprise the entire program.
This option performs optimization assuming that the files to be compiled comprise the entire program.  | 
The compilation is performed assuming that the following conditions are met. Operation is not guaranteed if these conditions are not met.  | 
The values and addresses of extern variables defined in the files to be compiled will not be modified or referenced from outside those files.  | 
Even if a file to be compiled calls a function defined outside the files to be compiled, the called function will never call a function in the files to be compiled.  | 
If this option is specified, it is assumed that the -Xintermodule option is specified.  | 
To perform optimization assuming that the files to be compiled comprise the entire program, describe as:  |