This option outputs the static analysis information file.
The static analysis information file is not output.
This option specifies the location where the static analysis information file to be generated during compilation as path.  | 
If an existing folder is specified as path, the static analysis information file is saved under the C source file name with the extension replaced by ".cref" to path.  | 
If an existing file name is specified or a non-existing folder or file name is specified, the static analysis information file is output with path as the file name when one static analysis information file is output.  | 
If two or more files with the same name (even if they are in different folders) are specified as source files, then a warning is output, and a static analysis information file is only saved for the last source file to be specified.  |