| 
 -change_message [V1.07.00 or later] 
 | 
This option changes specified warning messages into error messages.
[Specification format]
-change_message=error={num|num1-num2}[, ...]
 | 
 
[Detailed description]
-  | This option changes specified warning messages into error messages.  | 
 
The message numbers that are targeted by this option are W0510000 to W0549999.
-  | Specify the rightmost 5 digits of the message number as num, num1, and num2.  | 
 
If num1-num2 is specified, it is assumed that error numbers within the range have been specified.
-  | If num or num1-num2 is omitted, all target warning messages are changed into error messages.  | 
 
-  | When this option is specified more than once, all specifications will be valid.  | 
 
-  | If a message number that does not exist is specified, the specification is ignored.  | 
 
For message numbers, see "10.  MESSAGE".
[Example of use]
-  | To change W0520000 to W0549999 into error messages, describe as:  | 
 
>ccrh -change_message=error=20000-49999 a.c 
 |