|
-Absolute_forbid [V2.01.00 or later]
|
This option suppresses link-time optimization in a specific address range.
[Specification format]
-Absolute_forbid=range [, ...]
range := address[+size]
|
- | Interpretation when omitted |
None
[Detailed description]
- | This option suppresses link-time optimization in a specific address range. |
- | Specify the range in which you wish to suppress link-time optimization with address and size. Optimization will be suppressed for the sections included in the range of "address + size". |
- | Specify address and size as hexadecimal values from 0 to ffffffff. |
- | If +size is omitted, it is assumed that +0 was specified. |
- | If this option is specified more than once, all specifications will be valid. |
- | A warning will be output and this option ignored in the following case. |
- | When the -nooptimize option is specified |
[Remark]
- | When the range specified by this option overlaps with overlaid sections specified by the -start option, optimization will be suppressed for all overlaid sections in the overlapped area. |
To suppress optimization of only specific sections, use the -section_forbid option.
[Example of use]
- | To suppress link-time optimization in the range of addresses 0x1000 to 0x11ff, describe as: |
>rlink a.obj b.obj -optimize -absolute_forbid=1000+200
|