|
-AVOID_SADDR_STACK [V1.15.00 or later]
|
This option sets the stack area to an area excluding the SADDR area.
[Specification format]
- | Interpretation when omitted |
The range including the SADDR area is set for the stack area.
[Detailed description]
- | This option sets the __STACK_ADDR_START symbol and __STACK_ADDR_END symbol of the stack area to an area excluding the SADDR area. |
[Example of use]
- | To set the stack area to an area excluding the SADDR area, describe as: |
> rlink a.obj b.obj -device=dr5f10a6e.dvf -auto_section_layout -avoid_saddr_stack
|
[Remark]
- | If the -form={object|relocate|library} or -strip option is specified, this option will be invalid. |
- | If the -device option is not specified, this option will be invalid. |