3.6.1
Structure of the Motorola S-record file
The Motorola S-record file consists of seven recordsNote 1: S0 record as the header record, S1, S2, and S3 records as the data record, and S9, S8, and S7 records as the termination recordsNote 2.
Note 1. | Each record is output in ASCII code. |
Note 2. | The Motorola S-record files are divided into three types: 16-bit address type, (24-bit) standard address type, and 32-bit address type. The format of the 16-bit address type consists of S0, S1, and S9 records, the format of the standard address type consists of S0, S2, and S8 records, and the format of the 32-bit address type consists of S0, S3, and S7 records. |
The structure and contents of the Motorola S-record file are shown below.
Figure 3.2 | Structure of Motorola S-record File |
Each record consists of the following fields.
Sx XX YY......YY SS NL
(1) (2) (3) (4) (5)
|
|
|
|
|
|
Record type
S0: S0 record
S1: S1 record
S2: S2 record
S3: S3 record
S4: S4 record
S5: S5 record
S6: S6 record
S7: S7 record
S8: S8 record
S9: S9 record
|
|
|
Record length
The number of bytes as 2-digit hexadecimal number of (3) + number of bytes expressed by "SS"Note.
|
|
|
Field
|
|
|
Checksum
The one's complement is obtained from the sum of the number of 2-digit hexadecimal bytes in the record except for Sx, SS, and NL, and the lower one byte of the one's complement is expressed as a 2-digit hexadecimal number.
|
|
|
Newline (\n)
|