|
|
|
|
__LINE__
|
Line number of source line at that point (decimal).
|
|
__FILE__
|
Name of source file (character string constant).
|
|
__DATE__
|
Date of translating source file (character string constant in the form of "Mmm dd yyyy"). Here, the name of the month is the same as that created by the asctime function stipulated by ANSI standards (3 alphabetic characters with only the first character is capital letter) (The first character of dd is blank if its value is less than 10).Note2
|
|
__TIME__
|
Translation time of source file (character string constant having format "hh:mm:ss" similar to the time created by the asctime function).Note2
|
|
__STDC__
|
Decimal constant 1 (defined when the -strict_std option is specified).Note1
|
|
__RENESAS__
|
Decimal constant 1.
|
|
__RENESAS_VERSION__
|
If the version is V.XX.YY.ZZ, this will be 0xXXYYZZ00.
Example) V.1.00.00 -> -D__RENESAS_VERSION__=0x01000000
|
|
__RL78__
|
Decimal constant 1.
|
|
__RL78_S1__
|
Decimal constant 1 (defined when S1 is specified by the -cpu option).
|
|
__RL78_S2__
|
Decimal constant 1 (defined when S2 is specified by the -cpu option).
|
|
__RL78_S3__
|
Decimal constant 1 (defined when S3 is specified by the -cpu option).
|
|
__RL78_SMALL__
|
Decimal constant 1 (defined when small is specified by the -memory_model option or when S1 is specified by the -cpu option while the -memory_model option is not specified).
|
|
__RL78_MEDIUM__
|
Decimal constant 1 (defined when medium is specified by the -memory_model option or when S2 or S3 is specified by the -cpu option while the
-memory_model option is not specified).
|
|
__CCRL__
|
Decimal constant 1.
|
|
__CCRL
|
Decimal constant 1.
|
|
__DBL4
|
Decimal constant 1 (defined when 4 is specified by the -dbl_size option).
|
|
__DBL8
|
Decimal constant 1 (defined when 8 is specified by the -dbl_size option).
|
|
__SCHAR
|
Decimal constant 1 (defined when the -signed_char option is specified).
|
|
__UCHAR
|
Decimal constant 1 (defined when the -signed_char option is not specified).
|
|
__SBIT
|
Decimal constant 1 (defined when the -signed_bitfield option is specified).
|
|
__UBIT
|
Decimal constant 1 (defined when the -signed_bitfield option is not specified).
|
|
__FAR_ROM__
|
Decimal constant 1 (defined when the -far_rom option is specified).
|
|
__CNV_CA78K0R__
|
Decimal constant 1 (defined when ca78k0r is specified by the -convert_cc option).
|
|
__CNV_NC30__
|
Decimal constant 1 (defined when nc30 is specified by the -convert_cc option).
|
|
__CNV_IAR__
|
Decimal constant 1 (defined when iar is specified by the -convert_cc option)
|
|
__BASE_FILE__
|
C source file name (character string constant).
Unlike __FILE__, the C source file name is returned even when used in an include file.
|
|
__STDC_VERSION__
|
Decimal constant 199409L (defined when the -lang=c and -strict_std options are specified).Note1
Decimal constant 199901L (defined when the -lang=c99 option is specified).
|
|
__STDC_HOSTED__
|
Decimal constant 0 (defined when the -lang=c99 option is specified).
|
|
__STDC_IEC_559__
|
Decimal constant 1 (defined when the -lang=c99 option is specified).
|