|
.ALIAS [V1.11.00 or later]
|
The .ALIAS directive sets information about a symbol.
[Syntax]
Symbol field
|
Mnemonic field
|
Operand field
|
Comment field
|
|
.ALIAS
|
alias, symbol-name
|
[; comment]
|
[Description]
- | This directive generates an alias of the symbol. |
- | The generated alias can be specified in the .PUBLIC directive. |
- | If a label name that does not exist in any module is specified for the symbol name, an error will occur. |
- | This directive must be described after the definition of the symbol specified by the symbol name on the operand. |
[Example]
To allow only the alias symA to be referenced from outside the module, specify as follows.
symB:
.PUBLIC symA
.ALIAS symA, symB
|
SECTION=
SYMBOL ADDR SIZE INFO COUNTS OPT
symA
00000120 0 none ,g 0
symB
00000120 0 none ,l 0
|