6.2.2
Symbols generated by option specifications
The optimizing linker generates the following symbols using option specifications.
Table 6.2 | Symbols generated by option specifications |
|
|
|
|
|
-hide
|
$CNCL_n
n : 1 - 4294967295
Example) $CNCL_1
|
The local symbol name in the output file is changed to $CNCL_n.
|
|
-user_opt_byte
-ocdbg
|
.option_byte
|
The section name ".option_byte" is generated when the device file is specified with the section name ".option_byte" not existing in the source file. Note that the user option byte value and control value for on-chip debugging operation are set in the above section.
|
|
-security_id
|
.security_id
|
The section name ".security_id" is generated when the device file is specified with the section name ".security_id" not existing in the source file. Note that the security ID value are set in the above section.
|
|
-device
|
__STACK_ADDR_START
__STACK_ADDR_END
|
A consecutive area not used in the RAM area acquired from the device file is searched for and the following values are set to __STACK_ADDR_START and __STACK_ADDR_END.
__STACK_ADDR_START: Maximum address of the area + 1
__STACK_ADDR_END: Minimum address of the area
However, if the -SELF, -SELFW, -OCDTR, -OCDTRW, -OCDHPI, or -OCDHPIW option is specified, the area is set from the RAM area excluding the saddr area.
|
|
__RAM_ADDR_START
__RAM_ADDR_END
|
The RAM area is acquired from the device file, and the following values are set to __RAM_ADDR_START and __RAM_ADDR_END.
__RAM_ADDR_START: Start address of RAM area
__RAM_ADDR_END: End address of RAM area + 1
|
|
-debug_monitor
|
.monitor1
.monitor2
|
When the device file is specified while section names ".monitor1" and ".monitor2" do not exist in the source file, section names ".monitor1" and ".monitor2" are generated.
|
|
-rrm
|
.rrm
|
[V1.13 or later] If section name ".rrm" does not exist in the source file, section name ".rrm" is generated.
|