< Optimizing Linkage Editor (rlink) Options / Input Options >
If this option is not specified, the prelinker is initiated.
The prelinker supports the functions to generate the C++ template instance automatically and to check types at run time. When the C++ template function and the run-time type test function are not used, specify the noprelink option to reduce the link time.  | 
If form=lib or form=rel is specified while the C++ template function and run-time type test are used, do not specify noprelink.  |