4.1.7  
Conforming Language Specifications
 
(1)  | C Language Specifications (When the lang=c Option is Selected)  | 
 
ANSI/ISO 9899-1990 American National Standard for Programming Languages -C 
(2)  | C Language Specifications (When the lang=c99 Option is Selected)  | 
 
ISO/IEC 9899:1999 INTERNATIONAL STANDARD Programming Languages - C
However, variable length arrays are excluded.
(3)  | C++ Language Specifications (When the lang=cpp Option is Selected)  | 
 
Based on the language specifications compatible with Microsoft® Visual C/C++ 6.0