Clears the error state of a stream input/output file.
[Format]
#include <stdio.h>
void clearerr (FILE *fp);
[Parameters]
fp  File pointer
[Remarks]
The clearerr function clears the error indicator and end-of-file indicator for the stream input/output file indicated by file pointer fp.