The address condition and pass count condition [Simulator] for execution-related events you have set can be edited.
Perform this operation in the Detail dialog box (for execution events) that is opened by selecting [Edit Condition...] from the context menu after moving the caret to an execution-related eventNote you want to edit on the Events panel.
An execution-related event refers to any one of the following events in the Events panel.  | 
Execution-related event as start and end condition in detailed information on Performance Measurement event  | 
For the execution-related events that were set according to the descriptions in 2.11.3.1 Set a breakpoint, 2.11.4.1 Set a break event (execution type), 2.14.3.1 Set a Trace event, 2.15.2.1 Set a Timer Result event, and 2.16.1.1 Set a Performance Measurement event the initial values of the address and pass count conditions are listed below.