The display format of the address area/memory value area/character strings area can be changed using buttons below on the toolbar.
| The following buttons to change the notation of memory values are displayed. | ||
| The following buttons to change the notation of sizes of memory values are displayed. | ||
| Displays memory values in 16-bit width. Values are converted depending on the endian of the target memory area. | ||
| Displays memory values in 32-bit width. Values are converted depending on the endian of the target memory area. | ||
| Displays memory values in 64-bit width. Values are converted depending on the endian of the target memory area. | ||
| The following buttons to change the encoding of character strings are displayed. | ||
| Displays character strings as a half-precision floating-point value. | ||
| Displays character strings as a single-precision floating-point valueNote. | ||
| Displays character strings as a double-precision floating-point valueNote. | ||
| Displays character strings as a complex number of single-precision floating-pointNote. | ||
| Displays character strings as a complex number of double-precision floating-pointNote. | ||
| Displays character strings as an imaginary number of single-precision floating-pointNote. | ||
| Displays character strings as an imaginary number of double-precision floating-pointNote. | ||
| The following buttons to change the display format are displayed. | ||
| Opens the Scroll Range Settings dialog box to set the scroll range for this panel. | ||
| Opens the Column Number Settings dialog box to set the number of view columns in the memory value area. | ||
| Opens the Address Offset Settings dialog box to set an offset value for addresses displayed in the address area. | ||
| For details on the display of a floating-point value, see the section for the Memory panel. | 
 Hexadecimal
Hexadecimal Signed Decimal
Signed Decimal Unsigned Decimal
Unsigned Decimal Octal
Octal Binary
Binary 4 Bits
4 Bits 1 Byte
1 Byte 2 Bytes
2 Bytes 4 Bytes
4 Bytes 8 Bytes
8 Bytes ASCII
ASCII Shift_JIS
Shift_JIS EUC-JP
EUC-JP UTF-8
UTF-8 UTF-16 Big-Endian
UTF-16 Big-Endian UTF-16 Little-Endian
UTF-16 Little-Endian UTF-32 Big-Endian
UTF-32 Big-Endian UTF-32 Little-Endian
UTF-32 Little-Endian Half-Precision Float
Half-Precision Float Float
Float Double
Double Float Complex
Float Complex Double Complex
Double Complex Float Imaginary
Float Imaginary Double Imaginary
Double Imaginary Settings Scroll Range...
Settings Scroll Range...