Connect a host machine and E20.  If required, connect a target board, too. 
See E20 User's Manual for details on the connection method.
Figure 2.3  | Connection Example [E20]  | 
 
Caution  | Only serial communications are supported as the communication method with the target board (JTAG communications is not available).  |