This trace operation can be configured in the [Trace] category on the [Debug Tool Settings] tab in the Property panel.
Select whether to clear (initialize) the trace memory before tracing starts in this property.
Select [Yes] to clear the memory (default).
You can forcibly clear the trace memory when clicking the |
Select the operation after the trace memory is full with the collected trace data, from the following drop-down list.
The trace memory size is 128K frames (fixed).
|
Continues overwriting the older trace data after the trace memory is full (default). When the [Clear trace memory before running] property is set to [Yes], at the time of a resumption, trace data is collected after clearing the trace memory. |
|
|
When the trace memory is full, CS+ stops writing trace data (the program does not stop execution). |
|
|
When the trace memory is full, CS+ stops writing trace data and the program stops execution. |
Specify the frequency division ratio of the counter to be used for time tag display (i.e. display of the [Time] item in the Trace panel) (default: [1/1(4ns/0.3min)]).
Values in "()" on the drop-down list indicate the resolution and the maximum measurement time. |
button in the toolbar in the