2.17.7.2
Types of events that can be set or removed during execution
Types of events that can be set or removed during execution of the program or during execution of the tracer/timer are as follows:
Table 2.26 | Types of Events that Can Be Set or Removed during Execution |
|
|
|
|
|
|
|
Software break
|
|
|
|
Hardware break (execution-related: before execution)
|
|
|
|
Break event (execution-related: after execution)
|
|
|
|
Break event (access-related: Read, Write, Read/Write)
|
|
|
|
Trace (trace start, trace end)
|
|
|
|
Point trace
|
|
|
|
Timer result (timer start, timer end)
|
|
|
|
Action (Printf event)
|
|
|
|
Action (Interrupt event)
|
|
|
: Possible
: Possible if program execution is momentarily halted
: Impossible during tracer execution
: Not supported
: Impossible
Note 1. | Internal RAM area only |
Note 2. | Events cannot be set while the microcontroller is in a power-down mode. |