The program in execution can be stopped at the arbitrary position by setting a breakpoint. A breakpoint can be set with a single click of the mouse.
You need to configure the type of breakpoints to use before setting a breakpoint.
This section describes the following.
2.10.2.1 Set the type of breakpoints/break timing to use [E1] [E20]
2.10.2.3 Edit a hardware breakpoint
[E1/E20 [RX630, RX631, RX63N, RX63T, RX210, RX110, RX111, RX113, RX634, RX130, RX13T and RX26x Groups]]  |