The following types of CS+ execution functions are provided.
Select any of the following operations according to the purpose of debugging.
See "2.10 Stop Programs (Break)" for details on how to stop the program in execution.
2.9.2.1 Execute after resetting microcontroller (CPU)
2.9.2.2 Execute from the current address
2.9.2.3 Execute after changing PC value
You can automatically overwrite the value of I/O register/CPU register with the specified values before executing the program (see "2.18 Setting Up the Hook Process" for details).  | 
The PC value can be displayed in the status bar at any update interval during program execution. (See "(e) Current PC position".)  |