2.21.3  Icons for invalid input
 
In some of the dialogs provided by CS+, the  icon will appear at a point where incorrect characters are entered as a warning sign.
 icon will appear at a point where incorrect characters are entered as a warning sign.
| 
Remark | Placing the cursor over the  icon will pop up the information that indicates the characters to be entered. |