This dialog box is used to select a file-encoding.
| 
Figure A.6 | Encoding Dialog Box | 
 
This section describes the following.  
[How to open]
| 
- | From the [File] menu, open the Open File dialog box by selecting [Open with Encoding...], and then click the [Open] button in the dialog box. | 
[Description of each area]
Select the encoding to be set.
The encoding of the selected file is selected by default.
[Function buttons]
|  |  | 
| 
OK | 
Opens the selected file in the Open File dialog box using a selected file encoding. | 
| 
Cancel | 
Not open the selected file in the Open File dialog box and closes this dialog box. | 
| 
Help | 
Displays the help for this dialog box.  |