This panel allows you to view the information on and change the setting for the node selected in the Project Tree panel.
The following items are explained here.
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View], and then select [Property] from the [View] menu.  | 
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View], and then select [Property] from the context menu.  | 
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View], and then select [Property] from the [View] menu.  | 
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View], and then select [Property] from the context menu.  | 
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Device Top View], and then select [Property] from the [View] menu.  | 
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Device Top View], and then select [Property] from the context menu.  | 
If this panel is already open, selecting a different [Pin View] in the Project Tree panel changes the content displayed accordingly.  | 
If this panel is already open, selecting a different [Device List View] in the Project Tree panel changes the content displayed accordingly.  | 
If this panel is already open, selecting a different [Device Top View] in the Project Tree panel changes the content displayed accordingly.  | 
This area allows you to view the information on and change the setting for the node selected in the Project Tree panel.
The content displayed in this area differs depending on the node selected in the Project Tree panel.
In this panel, following tabs are contained (see the section explaining each tab for details on the display/setting on the tab).