|
csplus.is_timer_supported
|
This function checks if the timer provider that is currently selected supports the timer function.
[Specification format]
csplus.is_timer_supported(session_id)
|
[Argument(s)]
|
|
|
|
session_id
|
This argument is ignored in this version.
|
[Return value]
If the selected timer provider supports the timer function : True
If the selected timer provider does not support the timer function : False
[Detailed description]
- | This function checks if the timer provider that is currently selected supports the timer function. |
[Example of use]
>>> csplus.get_timer_providers()
{'csplus.timer': 'Time Measurement'}
>>> csplus.select_timer_provider("csplus.timer")
>>> csplus.is_timer_supported('0')
True
|