|
csplus.add_event_listener
|
This command adds the specified listener to the list of functions to be called when an event happen in CS+.
[Specification format]
csplus.add_event_listener(listener)
|
[Argument(s)]
|
|
|
|
listener
|
A function which accept a String parameter.
|
[Return value]
None
[Detailed description]
- | The function has format function_name(string_parameter) |
- | The value which will be passed to the String parameter of listener has the format debugger_state;0;event. |
|
|
|
|
debugger_state
|
A fixed string indicating that the event is related to debug activity.
|
|
event
|
The name of the event. The information has one of following value:
Program is downloaded: downloaded
Debug session is reset: reset
Debug session is about to resume: resuming
Debug session is suspended: suspended
|
[Example of use]
>>> def listener1(event): print("Listener 1: " + event)
...
>>> csplus.add_event_listener(listener1)
>>> csplus.download_loadmodule(session_id)
>>> Listener 1: debugger state;0;reset
Listener 1: debugger state;0;resuming
|