Appendix Contents of Information List Panel

Below chart describes contents of Variable List Panel. For the details, refer to help.
"Static" information is described after build. "Dynamic" information is described after connecting the debug tool.
|
Description |
Overview |
Static/Dynamic |
|
Variable Name |
Name of the variables defined/referenced in C source |
Static |
|
File Name |
File name of C source file where the variable is defined |
Static |
|
File Path |
Name of the function where the variable is defined |
Static |
|
Import |
Source of the variable information |
Static |
|
Attribute |
Variable's symbol attributes/symbol-modifier attributes |
Static |
|
Type |
Type of the variable |
Static |
|
Members |
Members of the structure/union |
Static |
|
Address |
Variable's allocated address |
Static |
|
Size |
Size of the variables |
Static |
|
Reference Count |
Number of times the variable is referenced in the program |
Static |
|
Read Count |
Number of times the variable was read |
Dynamic |
|
Write Count |
Number of times the variable was written |
Dynamic |
|
Read/Write Count |
Number of times the variable was read/write |
Dynamic |
|
Minimum Value |
Minimum value stored in variables |
Dynamic |
|
Maximum Value |
Maximum value stored in variables |
Dynamic |
|
Data Coverage |
Data coverage ratio of the variable |
Dynamic |
|
Total |
Total of above item in the target file |
- |