| [General - Project] category | 
Use this category to configure general settings relating to the project.
| 
Figure A.44 | Option Dialog Box ([General - Project] Category) | 
 
The following items are explained here.
[How to open]
| 
- | From the [Tool] menu, select [Options...]. | 
[Description of each area]
| 
(1) | [Confirm whether to reload when the project is externally modified] | 
|  | 
Monitors opened project files and subproject files for changes. When there is a change, a Message dialog box confirming whether to reload the file is displayed (default). | 
|  | 
Monitors opened project files and subproject files for changes. However, even when there is a change, no Message dialog box is displayed. | 
| 
(2) | [Output the common project file for e2 studio too when the project is saved] | 
|  | 
Outputs the common project file for e2 studio too when the project is saved (default). | 
|  | 
Does not output the common project file for e2 studio when the project is saved. | 
| 
Remark | The output of a common project file (*.rcpe) is available with a project for CC-RL, CC-RX, or CC-RH but is not available with a project for GHS CCRH850 or a debug-dedicated project. | 
| 
(3) | [Set default value as "Share settings among users" to [Type of storage and sharing environment-dependent information] property on creating project] | 
|  | 
Sets the initial value as [Share settings among users] for the [Type of storage and sharing environment-dependent information] property when the project is created.] | 
|  | 
Sets the initial value as [Save for each user] for the [Type of storage and sharing environment-dependent information] property when the project is created (default). | 
| 
Initialize Settings | 
Returns all currently displayed setting to their default values. | 
[Function buttons]
|  |  | 
| 
Initialize All Settings | 
Restores all settings on this dialog box to their default values. 
Note, however, that newly added items in the [General - External Tools] category will not be removed. | 
| 
OK | 
Applies all setting and closes this dialog box. | 
| 
Cancel | 
Ignores the setting and closes this dialog box. | 
| 
Apply | 
Applies all setting (does not close this dialog box). | 
| 
Help | 
Displays the help of this dialog box. |